Hi Team,
I’m using the TPS7A2028 and I really like it. I’m currently powering the dispenser with 3 alkaline batteries (1.5VDC each, 4.5VDC total) in series. There is a possibility that I may move to 4 alkaline batteries. That would be a total of 6.0VDC. However, all new alkaline batteries are overcharged to 1.6VDC, which makes the total 6.4VDC for a short time. The absolute Vin for the TPS7A2028 is 6.0VDC. Is there some fudge factor there? Could it handle the overcharge? If not, is there an LDO with similar specs that could handle 4 alkaline batteries?
Thanks!
Connor