Other Parts Discussed in Thread: LM74800-Q1, LM74502,
I have a switch power that outputs 54V/14.8A
I used the LM74700 Ideal Diode Controller because it needs to be used in parallel, but I have a question about ovp
HI SIR
OVP protection specification is as follows
1:latch
2:125% (min) output V
If I Set 125% output V so that the LM74700 ANODE pin voltage will exceed 65V max
Do you have any suggestions to solve the OVP problem?