Other Parts Discussed in Thread: USB-PD-CHG-EVM-01, , BQ25792
Hi Team,
Currently, our customer are evaluating the following conditions.
Source: 45W PD adapter
Sink: USB-PD-CHG-EVM-01
Tool: Advance configuration of Application_Customization_Tool ver7.0.3
They would like to set 20V/2.25A so know the proper Sink PDO setting.
I understand the following setting.
Is my understanding correct?
[Our settings]
Sink PDO1 15W (5V*3A)
Sink PDO2 27W (9V*3A)
Sink PDO3 45W (20V*2.25A)
[PDO3 setting picture]
Regards,
Hide