Other Parts Discussed in Thread: BQ40Z50
Hello,
I made several 4S7P Li-ion battery packs with a capacity of 21Ah each, using the BQ40Z50 as BMS.
Now I'm required to provide a 42Ah pack and I wonder if it is possible and safe to connect two of the previous packs in parallel, which means to short the outputs and the communication buses of the packs, while each one has it's own BQ40Z50 as BMS.
If so, what am I required to do besides making sure that the packs' voltages are identical before I connect between them?
Besides this proposal being more versatile, I'm aware of the 32,767mAh capacity limit of the BQ40Z50.
Best Regards!
Itay