Other Parts Discussed in Thread: TPS7A02,
Hi,
I am using the TPS7A20285 LDO and simulating the effect of ESR of the output cap.
I see the datasheet lists the output cap requirements as 0.47uF minimum and 100mohm max.
I downloaded the spice model on the product page and I did some simulations but I am not sure the model shows me the effect of output cap on the loop stability.
Since the model seems to be a generic model I think they only thing I had to modify was the V_out parameter (set to 2.85V in my case) but maybe I need to modify other parameters?
I attached my sim results which would show very stable response with 1mohm (dashed line) or 1 ohm (solid line), I tried with higher resistance (ESR) and it does not change much either. Can you check if the model includes this behavior, if not, do you have more details about the behavior with higher ESR? my application will be on the edge of the ESR limit and possibly even the cap min capacitance limit, I want to see how much margin I might have.
I will have the same question for the TPS7A0218 but that datasheet does not specify the min or max ESR, does it mean there is no limitation?
I already had a discussion with "Customer support" but they told me that EE support is a better forum for this, in caser you want to see here is the case #
Case Number: CS1189132
Thanks, LV