The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563208: Help with overcoming negative Inductor current

Part Number: TPS563208

When testing the controller for 12V Input to 5V, 1A output I noticed negative Inductor current till 0.6 - 0.7 A output current load. I have used the typical values of the Inductor (3.3uH) and output Capacitor (10uF+10uF+0.1uF) that was mentioned in the datasheet. How do I overcome this and also how can I find Bandwidth of the controller? 
Thanks.