Hello,
I’m looking for some help debugging a design that uses TPS65981ABIRTQR. The intended setup is to have it as a UFP Power Sink which controls an HD3SS460IRHRT and acts as a mux for SBU and USB 2.0 lines.
Design: See below pictures
Issue: When we connect it with a DFP Source, the VBUS voltage oscillates between 1.1 V and 0.5 V, and there is audible clicking coming from the TPS65981ABIRTQR. I’m assuming this means that one of the gates is continuously opening but an issue is occurring, or the power from the source is being rejected. When we apply 5 Volts independent of the USB-C supply to Vbus, there is no clicking but the device is still not operating as expected so I assume that the aforementioned gates is staying open after the initial application of power.
Current changes made:
- BUSPOWERZ has been connected to GND through 120k resistor (done after issue was noticed)
- CCn have been connected to their respective RPD_Gn pin to allow boot from no power
- PP_5V0 and PP_CABLE have been disconnected from GND and connected to 5V0 (no effect on the issue)
I don’t believe the software is causing this issue as the power cycling is occurring quickly and does not reach a high enough voltage to allow the SPI flash to be read from.
Thank you.