This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92410: Maximum output power

Genius 16850 points
Part Number: TPS92410
Other Parts Discussed in Thread: TPS92561

Hi Experts,

My customer is looking an LED driver for up to 150W driving, stack voltage up to 170V.

I am seeing these parts:

The customer requirement is actually for 4 different watt.
Those are 60W , 80W ,100W,150W. Can arrange led pieces according to driver chip.
It can be 170V -0,35A for 60W.

Can these will work for such amount of power?

Thanks for your confirmation.

Regards,
Archie A.