Hi Team,
I am trying to understand the worst case maximum voltage that RESET will trip when using a fixed 5V0 setting.
I see in the datasheet that the max falling voltage is 95%:
My question is if this accounts for DC accuracy of the 5V0 rail or not.
To clarify further the FB pin has the following tolerance:
So will the worst case maximum voltage RESET trip at 5.075*0.95=4.821V or is DC accuracy accounted for in 95% spec and the worst case maximum RESET trip at 5.0*0.95=4.75V
Best,
David