Dear Teng, please answer
I see, that common-mode input voltage range for amlifiers is minus 0,3 to Vcc-2V (section 7.7 of the datasheet). I have Vcc= 12 V.
QUESTION: Can I set a voltage drop 0,05 V on the R13 with the same circuit, which is given in the datasheet in 10.2.2.2.3 section?
I will, of course, change the values of the resistors R1, R2, R13. I need 4 A output current. Vout = 4 V.
TIA
Sincerely,
Vladimir Naumenkov