Other Parts Discussed in Thread: BQ24192
Hello,
I have one more question regarding BQ27531-G1 : Cycle count.
As per the BQ27531-G1 TRM , one cycle occurs when accumulated discharge ≥ CC Threshold. In our CC Threshold=4000mAh (which is normally set to 90% of the design capacity ,4400mAh). When the gauge accumulates enough discharge capacity equal to CC Threshold, it increments CycleCount() by 1. When I performed discarging and charging of battery, cycle count has increased to 1.
But I observed that, when I keep the device with continuous charging state then also gas gauge increments the cycle count. It should not happen, right? as I am not discharging the battery. Why this is happening?
Also when I kept the device continuosly ON with continuous power adapter, after 8 days device generates a gas gauge error.
Waiting for your reply.
Regards,
Janhavi Rane