Other Parts Discussed in Thread: TPS61040
Hi,
we are using the TPS61040-Q1 Boost converter for converting the 3.3V to 6V. Please find the schematics
Attached the power sequence of this converter
The Yellow color represent the input voltage which is 3V3. The green color represent the (TPS61040-Q1) Boost output which is 6V0. This 6V0 is going to input of LDO(LOAD) which output is 5V0. The Violet color represent the Load current of Boost
Here we can see that the the TPS61040-Q1 output voltage is drop when the LDO turn on.
Could you please give the solution for the same as earliest possible.
Thanks & Regards,
Thangaprabu S