Hi Team,
I am curious about the input voltage and output voltage of TPS563231;
Why the device cannot work if it exceeds input range 4.5 ~ 17V range ?
Why can only output a voltage of 0.6 ~ 7V? If the feedback of the regulation is not in this range, what will happen?
When input voltage is 17V. and the max duty cycle is 87%, it can output 13.28V, right?