This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24720: TPS24720 -Request for Design Support

Part Number: TPS24720
Other Parts Discussed in Thread: TPS25985, CSD16401Q5

I have planned to use TPS24720 Hot Swap controller in one of my project.
Below Listed my design requirement

Input Operating Voltage: VIN(NOM) :12V
Upper UVLO Threshold : 10.04V
Lower OVLO Threshold : 13.45
Maximum Load Current: IOUT(MAX ) :30A
Target Current Limit :33A
Fault Response :Latch Off
Please suggest suitable N channel MOSFET for My application ?

I have attached TPS24720 Hot Swap Design Tool calculation.
Could please verify all points and provide your feedback if any

Thanks 
Sujith