Part Number: BQ24190
Other Parts Discussed in Thread: BQ25601D, , BQ25611D
Hi Team,
A customer is looking to charge a single 3500ma cell in a sealed end product from either USB port or adapter. They only need to use a single connector (USB A to micro) to connect to the charging choices.
The rest of the requirements are:
-No dual input
-need BC1.2 primary detection
-Must have DP/DM detection
-Can automatically select 500ma/1.5A USB charge
-No need for OTG while the charger is hooked up
Will BQ24190 work? If not, can you suggest another part device that would work best?
Thanks!
Regards,
Marvin