Hi Expert
in the EVM:
1. my customer change the parameter is:
Roff: 1K
Coff: 470pf
RSNS: 75mohm
EN PWM: 140HZ
PWM min pulse: 5uS
min stable current: 385mA
customer used internal PWM method, control EN pin.
situation: When external PWM(control EN) reduce to 130HZ, circuit output will close.
Question 1:the relationship with EN PWM frequency with output current? do you have equation to explain it?
Question2: when used EN control mode, device will use internal PWM, could you please tell us the internal control frequency?
Queation3: we want to optimization output current rise and fall time, do you have any guide to optimize it?