Other Parts Discussed in Thread: TPS62933P, TPS54308,
Hello,
I have designed a DC/DC converter (TPS5405DR) and used it on one of my boards.
At low load (<100mA) I now have a Pk-Pk voltage of 170mV with a frequency of 29k Hz.
At a load of about >400mA the Pk-Pk voltage suddenly drops below 20mV.
Attached is the schematic including the layout. On the two internal layers
there are two GND planes.
How can i improve the ripple during low load conditions?