Hi Sir/Madam,
i check the TPS7A25 datasheet.
i have a source 12Vdc. output around 3.3 V / 1A.
1.
T A(MAX) = T J(MAX) – (R θJA × P D )
T A(MAX) =125°C – [73.3°C/W × (12 V – 3.3 V) × 0.09 A] = 70.2°C
does it mean the contact max thermal of TPS7A2533 is 70 °C ???
2.
i measure the contact thermal of TPS2533 in my system. it's around 105°C.
T J = R θJA × P D + T A
= 73.3°C/W × (12 V – 3.3 V) × 0.09 A +105
= 162 °C.
could you suggest how to solve this problem? or change another LDO (pin to pin)
thanks.