Other Parts Discussed in Thread: UCD7242,
On our last build of PCAs, the UCD9246 power controller is losing control of the DPWM-1a output. Either at powerup, or with a slight freeze spray the DPWM-1a goes from 12.5% duty cycle (1.5V output from 12V) to 50%. This causes the UCD7242 driver to boost the 1.5V output, current goes from 0.5A to 10A+, and the UCD7242 FLT asserts. The UCD9246 DPWM-1a stops and the whole controller shuts of per it's fault programming. This part has been in stready use for 12 years and this seems lot related. Can you contact me and help with this issue?