Other Parts Discussed in Thread: UCC28951, UCC2895, CSD19536KCS,
Good morning,
I am designing a 1.5kW phase shift bridge converter with a variable output voltage between 5V and 45V.
My intention is to use the UCC2895 for this. (Note: I do not want to use the UCC28951 in this application)
Power output reduces as the output voltage reduces.
Maximum power is only possible at 45V output.
I would like to use the UCC24624D for controlling your CSD19536KCS MOS FETs on the output as synchronous rectifiers.
The variable voltage is a problem for powering the UCC24624D.
I could provide a separate fixed regulated voltage feeding the UCC24624. What is your opinion on this?
Otherwise I could use a pulse transformer circuit driving the synchronous rectifiers from the signals on the primary side.
My only concern is when the converter enters DCM.
Can the synchronous FETs really be damaged when using the pulse transformer circuit in SLUU109B?
Thank you.