This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524P-Q1: How to program PMIC permanently?

Part Number: LP87524P-Q1
Other Parts Discussed in Thread: IWR6843, LP87524J-Q1

Hi, i have been using TPS87524q1 evaluation board for my Project where I am using IWR6843. IWR6843 operating voltages are 3.3V,1.2V,1V and 1.8V. The evaluation board which I have bought default voltages are 3.3V, 1.2V,1.8V and 2.3V. I have been programming it to get the voltages required for IWR IC and observed that it is OTP, is there any solution that I can change the default program permanently so that the values will not change even after power off.

Thank you