Other Parts Discussed in Thread: BQSTUDIO,
Hello,
For PbA, the taper method is used (FC Set %=-1) for detecting a Full Charge.
The TRM pg60 places great importance on the timing of charge cut-off using criteria a,b,c as stated here:
However, the TRM pg31 states the criteria differently here:
Please clarify for PbA and suggest the BQSTUDIO watch window parameters for supporting a proper charge cut-off.
Also please note, that for PbA there is a phase 1 charge voltage and a phase 2 charge voltage.
I find only the cell charge voltage T#-T# parameters defined in the DF Configuration>Data section.
Which charge voltage is used here for PbA?
If this is to define the phase 1 voltage, then where is the phase 2 voltage defined?
Sincerely,
Rom