Dear team,
From the specifications of TPS7A8300ARGWR and TPS7A8300RGRR, it can be seen that the packages of these two materials are the same. Can these two materials be replaced?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
What is the question here? These parts are functionally the same, but they have different packages that are different sizes one is a 5x5 QFN and one is a 3.5x3.5 QFN, so they are not p2p. So you can use them if you are willing to redo the layout, but you cannot use the same footprint for both. Hope this helps.
Regards,
Mark