Part Number: LM3643
Hi team,
1. if the TX is high forever, do this mean we can't enter flash mode right?
2. what would happen if TORCH/TEMP and STROBE both high, what will IC react base on if I2C enable register is torch mode ?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM3643
Hi team,
1. if the TX is high forever, do this mean we can't enter flash mode right?
2. what would happen if TORCH/TEMP and STROBE both high, what will IC react base on if I2C enable register is torch mode ?
thanks
hi Fred
1. yes, when TX is high, it will be forced into torch mode.
2. do you mean in the following register, Bit5 is 0, Bit 4 is 1, Bit 3 is 10?

HI Mason,
1. can they connect HWEN STROBE and TORCH/TEMP pin together and pull high? since they can't place via under the package in this kind of PCB, so they need give HWEN a trace out of package.
2. I mean TORCH/TEMP and STROBE "pin" are both high if bit5=1, bit4=1, bit3=10,
will it listen to hardware pin or I2C register?