This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD18543Q3A: Need Alternative part number

Part Number: CSD18543Q3A
Other Parts Discussed in Thread: CSD19537Q3

Hello there!

I need an alternative part number for  CSD18543Q3A N-channel MOSFET which is being used in switching regulators. I tried finding in mouser , digikey, TI and others but couldn't find the suitable footprint fit, so i need help.

The alternative part shall be: 

  •  Available in TI, Digikey, Mouser etc., with stock at least 50 units.
  • Mechanically fit i.e., footprint dimensions, because the board is already done and i need to solder it in place.
  • Electrically fit i.e., Vds & Ids

I have also attached the design where this part is used for reference.


DCDC-15V.pdf

Thanks in advance !.

  • Hello Arvidn m,

    Thanks for your interest in TI FETs. This CSD18543Q3A is our only 60V FET in 3.3 x 3.3mm SON package. The only other TI alternative in that type of package is the CSD19537Q3 (100V NFET, 14.5mΩ max at VGS = 10V) which should be footprint compatible with the CSD18543Q3A. I am fairly certain that there are similar offerings from TI's competitors but I am not familiar with their products and would suggest you use cross referencing tools available on their websites or at digikey/mouser, etc.

    Best Regards,

    John Wallace

    TI FET Applications