This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ769142: BQ769142: Coulomb Counter query

Part Number: BQ769142

Hi

I have two query need your help.

According to the TRM Table 4-6.

 

Assuming that userA is 1mA, a total of 10.7mah is used

1. After DASTATUS6() subcommand is issued, will there be a difference of + 10 or - 10 between 0-3 bytes due to charging and discharging? Or will + 10 be displayed?

2. The 4-7 byte decimal part? What value will 0.7mah get in 4-7 bytes of dastatus6()?

Waiting for your reply.

Thanks

Star