Hi,
I had two questions regarding the TPS7H1101A-SP device.
1) For calculating the RCS value, I am a little confused as to what to use for the Vcs value. I have a Vin = 2.5V and Vout = 1.8V with Iout = 1.2A. I am not sure what I should use for Vcs. Can you please help?
2) For the Power Good signal, it seems in the datasheet and on the eval boards that it is pulled up to Vout. Is this necessary? Can I pull it to Vin instead? The reason why I am asking is that on one of my designs I am feeding this signal to an enable and the power good line would only be pulled up to 1V which is too low for my enable input.
Thanks!
Jeff