Hi,
I can't find VIN-SW (HS FET Vds) spec in datasheet.
Do we spec the max voltage rating?
My customer measured -6.72 negative voltage on VIN-SW, is that OK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jim,
Are you within the recommended range with respect to IC GND for SW and VIN?
Typically we do not spec VIN to SW but at the same time we do not want it to be below ~-3V for more than few ns.
let's start with measuring VIN and SW to GND, can you provide that plot.
Also, let's make sure the measurement are done properly with Diff probe and short leads.
Thanks!
Tahar
Hi Jim,
I will close this post as long time no feedbacks.
If you need further support, please reply and this post will be open again.