Part Number: BQ24192
Other Parts Discussed in Thread: BQ27531-G1, , BQSTUDIO
Hello,
We are using BQ27531-G1 along with bq24192 charger. Our circuitry as follows:

As per the circuitry, rechargable Li-ion battery is connected to the BAT pin of bq27531-g1 gas gauge. External 5V power supply is connected to the VBUS pin of charger and SYS pin provides voltage to the system. During the test when device is on with external power supply, we observed in bqstudio that when FC bit set (battery capacity :100%) DSG bit also sets at the same time and it starts to discharge the battery for few mintues and then it clears both the bits and start to charge again.
From this test, we understand that when rechargeable battery is full , VBUS disconnect the connection with external power supply and system runs via battery. Did we understood correctly? is chager works like this when battery is full?
Regards,
Janhavi Rane