This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51632-Q1: Searching TI solution

Part Number: TPS51632-Q1


Hi team

There is a good new that we could DIN TI product!

Please help suggest TI solution, THX

This application is 5MP OMC , in addition, I2C needs to be able to report exceptions, and it also conforms to ASILB, THX

SPEC:

  1. input need support 4V~18V or higher
  2. VOUT 0.9V

  3. 2A min
  4. Synchronous
  5. Spread Spectrum
  6. AECQ
  7. ASIL B
  8. Frequency :2MHz up
  9. I2C