This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH12000W: Information about the temperature rating of the internal inductor

Guru 12410 points
Part Number: PTH12000W


Hi, 

I am using PTH12000W, but the temperature of the part surface is very high. In particular, the surface temperature of the inductor reaches 118°C.

Is it possible to tell me the rated temperature of the inductor? Also, if there is a rated temperature for the internal parts, please let me know.

Thanks,

Astro