Other Parts Discussed in Thread: TPS650330-Q1, LM26480
My application currently uses a TPS65708YZHR, which has a 5V input and creates required 3.3V, 1.8V, and 1.2 V rails. I'm trying to reduce the thermal profile of my device, and based on temperature measurements this PMC is the hottest component on my PCB. Are there alternate TI power management chips that can provide a lower thermal profile?