Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3988: Can Power Good (PG) really not go above VDD?

Part Number: LP3988

When I look at the Absolute Maximums section, it says that PD must be the lesser of VIN + 0.3 V or 6 V.

Is actually this correct? This seems unusual for an open-drain power-good output, that it can't go above the input rail.