Part Number: LP8869C-Q1
Hello,
in LP8869C-Q1 datasheet, we cannot find pacakge information.
https://www.ti.com/lit/ds/symlink/lp8869-q1.pdf
where we can find pacakge information, pin pitch, etc..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP8869C-Q1
Hello,
in LP8869C-Q1 datasheet, we cannot find pacakge information.
https://www.ti.com/lit/ds/symlink/lp8869-q1.pdf
where we can find pacakge information, pin pitch, etc..
Hi Suzuki-san,
The last pages are all about package information.

Br,Gracie
this does not show package size.
it shows only width: 6.5mm.
but, no information for length. i hope general pw package should be 6.4mm * 6.5mm.
where i can find 6.4mm from datasheet?
| Package family | TI package name | Description | Pin count | Pitch (mm) | Maximum height (mm) | Length (mm) |
|---|
| HTSSOP | PWP | Plastic Small Outline | 20 |
0.65
|
1.0 |
6.5
|
4.4
|
Hi
You could search on TI.com https://www.ti.com/packaging/docs/searchtipackages.tsp?packageName=SO to find this information.
Actually the drawing is provided in datasheet and that's enough normally.
BR, Gracie
thanks.
in datasheet, there are two thermal pad information. which is for LP8869QPWPRQ1?
on p39, thermal pad is 2.4/1.61 * 3.4/2.61 mm^2
on p41, thermal pad is 2.45/1.65 * 3.2/2.45 mm^2.
thanks.
in datasheet, there are two thermal pad information. which is for LP8869QPWPRQ1?
on p39, thermal pad is 2.4/1.61 * 3.4/2.61 mm^2
on p41, thermal pad is 2.45/1.65 * 3.2/2.45 mm^2.
this link does not show thermal pad infomration.
please tell us typ size for thermal pad.
on p39, thermal pad is 2.4/1.61 * 3.4/2.61 mm^2
on p41, thermal pad is 2.45/1.65 * 3.2/2.45 mm^2.
thanks. can you also tell me typ size for thermal pad? p40 or p42?
it is needed for CAD.
it is helpful. but, customer document work needs tharmal pad size.
could you please tell us size for thramal pad?
Hi Suzuki,
The previous datasheet screenshot has illustrated the thermal pad size: 3.7*2.4.
lp8869c-q1.pdf This datasheet has only one size for thermal pad.
Br, Gracie
Hi
thank you for your response. from P38, we can read 3.7*2.4.
what is the P37 mean? frm p37, i can get only thermal pad informaton. should p37 be removed?
suzuki
It's detailed information about thermal pad. It's TI trademark. You can look into the application brief for details.
i understand, but if there is number, it make complex. it makes misslead for my customer. can you change datasheet to make more clear?
No, Suzuki.
It's the right version TI standard datasheet. I think customer could understand the size and shape of thermal pad from this version. And I think it's unnecessary for more discussion.
BR, Gracie