This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3050EVM-001: BQ3050 Should Shutdown / Disconnect upon CUV

Part Number: BQ3050EVM-001
Other Parts Discussed in Thread: BQ3050, BQEVSW

Hello Team,

Is there any way where we can disconnect battery  during RUNTIME ( i.e. no SMbus Communication , No Battery Output Voltage ( Pack+/Pack-) , No Current ) from the Load upon certain condition Like CUV condition / Specific cell Voltage ?

Something Like Sleep / Shutdown , Not sure which one will fulfill above ?

Pls. also suggest steps to achieve this.

- Regards

  • Hello Bhupendra,

    CUV threshold can be set to turn off FET effectively providing no battery output voltage, no current. See 1st level protection features section.

    It does not make sense to turn off SMBus communication because the system needs to read SOC to determine whether it is safe to power on. I may help to understand th purpose of doing this.

  • Yes , But Turn OFF FET upon CUV is Not working. after CUV we get Voltage and current output even DSG FET is OFF.

    Here are the Voltages :

    Charge Time (81%)

    1. VPACK = 16.29V
    2. VDSG = 26.46V

    @Discharge on CUV

    1. VPACK = 12.85V
    2. VDSG = 12.45

    Vo(FET ON DSG) = 26.46 - 16.29 =  10.17V

    Vo(FET OFF DGS) = 12.45 - 12.85 = -0.4V

    All seems in Range , then why Still we see Load current flowing from battery after CUV Condition ?

  • Hello Bhupendra,

    Can you elaborate how you determine "load current flowing". Also is this on the EVM or on your design?

  • It is EVM Only. For Piloting we have used EVM with battery as BMS.

    We have connected LOAD to Battery using DMM in series with them to measure Load current from battery. Even after CUV Condition DMM shows same Load current flows through. 

    Here , is the Setup :  DMM = Digital Multimeter ( TRUE RMS ).

  • Hello Bhupendra,

    bq3050 implements JEITA. As a result the CUV is dependent on temperature.

    Is the CUV bit set in SafetyStatus? Can you send bqEVSW register flags screenshot?

  • Yes , CUV Flag sets upon crossing the threshold

    .

  • Thanks. CUV is triggered. The current is probably from another source. I would be looking at the hardware connections. Is a charger connected to the Pack? bq3050 only supports up to 4s. What was the previous mention of 26.46V?

  • Hello Shirish,

    Yes, Battery is connected in 4S only. Configuration is : 2p4S. ( Max :16.8V ). 

    Not sure why it shows : VDSG = 26.46V . May be some floating voltage noise. we measure two time @ DSG test point of EVM with reference to VSS and Pack-..

    Charge is not connected while discharge. In Our case , either it is charger can be connected OR Load.  

    FYI : we have same issue with Both EVM.

    - Regards

  • I would suggest tracing the source of the 26.46V. Since the gauge is seeing the same current, i would double check all connections to the EVM and see which points are above 20V.

  • Hello Shirish,

    We have checked all Test point provided on EVM board  But we see this 26.46V voltage Both at CHG and DSG FET Gate Terminal . Measure with respect to

    PACK- terminal using digital multimeter. Charging and Discharging works fine. From the Datasheet ( Page no 6 ) this voltage seems OK. 

    All TESTPOINT Measuring is as follow  ( Battery was Fully charge 100%) :  

    PACK + = 16.35V
    FUSE PIN = 0.05V
    VCC = 15.96V
    DSG = 26.5V
    CHG = 26.5V
    BAT = 15.90V
    2.5V = 2.246V
    3.3V = 3.332V
    Vout = 0.2V

    Thanks,

  • Hello Bhupendra,

    Is this with the charger disconnected?

  • Yes , All Data without Charger / Load connected.  

    While Battery is under relaxation. 

  • That is weird. We have not seen this before on the TI EVM. Can you try sending the FETControl command to turn off the FETs and see if it makes any difference?

    TRM section B.2 FETControl (0x46)

  • Hello Shirish,

    Manually , DSG FET Operated correct by reading software , i.e. bit set and RESET. 

    But as usual current flows when DSG FET shows OFF by BQEVSW.

    For More Insight attaching Discharge Log upto Cell Voltage < 3200mV ( LOAD Disconnected Manually after that ) , CUV Th = 3380mV.

    bq EVSW Version: 0.9.80 for bq3050 v0.02	
    Device: bq3050 R0, FW version: V0_02_BLD0003
    9/15/2022 10:53:18 AM	
               
    Design Capacity: 6900 mAH
    Design Voltage: 14400 mV
    Specification Info: 0031 hex
    Manufacture Date: 01-Jul-2022 
    Serial number: 0001 
    Manufacturer Name: SPARK 
    Device Name: bq3050               
    Device Chemistry: LION 
    
    Sample	Stamp	~Elapsed(s)	ManufAccess	RemCapAlarm	RemTimeAlarm	BattMode	@Rate(@)	@TimeFull	@TimeEmpty	@RateOK	Temperature	Voltage	Current	AvgCurr	MaxErr	RSOC	ASOC	RemCap	FullChgCap	RunTimeEmpty	AvgTimeEmpty	AvgTimeFull	ChgCurr	ChgVolt	BattStat	CycleCnt	CellV4	CellV3	CellV2	CellV1	FETStatus	SafetyAlert	SafetyStat	PFAlert	PFStat	OpStat	ChgStat	TempRng	PendEDV	ManuFacStat
    1	10:54:03 AM	0	0074	285	10	0081	0	65535	65535	1	25.95	16375	3	3	8	100	74	5101	5108	65535	65535	140	0	16500	00E0	9	4115	4108	4068	4084	0006	0000	0000	0000	0000	8040	0000	0004	13600	0000
    2	10:54:48 AM	45	0074	285	10	0081	0	65535	65535	1	25.95	16145	-2195	-685	8	100	74	5098	5108	139	389	65535	0	16500	00E0	9	4060	4053	4012	4017	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    3	10:55:33 AM	90	0074	285	10	0081	0	65535	65535	1	26.05	16083	-2193	-2157	8	100	74	5065	5108	139	141	65535	0	16500	00E0	9	4046	4038	3998	4002	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    4	10:56:18 AM	135	0074	285	10	0081	0	65535	65535	1	26.15	16068	-2193	-2189	8	99	74	5045	5108	138	138	65535	0	16500	00E0	9	4042	4034	3994	3998	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    5	10:57:03 AM	180	0074	285	10	0081	0	65535	65535	1	26.15	16056	-2192	-2192	8	99	73	5026	5108	138	138	65535	0	16500	00E0	9	4038	4031	3991	3995	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    6	10:57:48 AM	225	0074	285	10	0081	0	65535	65535	1	26.25	16034	-2190	-2191	8	98	73	4987	5108	137	137	65535	0	16500	00C0	9	4033	4025	3986	3990	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    7	10:58:33 AM	270	0074	285	10	0081	0	65535	65535	1	26.35	16024	-2189	-2189	8	98	72	4968	5108	136	136	65535	0	16500	00C0	9	4031	4022	3983	3988	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    8	10:59:18 AM	315	0074	285	10	0081	0	65535	65535	1	26.45	16004	-2186	-2187	8	97	72	4930	5108	135	135	65535	0	16500	00C0	9	4026	4017	3978	3983	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    9	11:00:03 AM	360	0074	285	10	0081	0	65535	65535	1	26.45	15995	-2186	-2186	8	97	72	4910	5108	135	135	65535	0	16500	00C0	9	4023	4015	3976	3981	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    10	11:00:48 AM	405	0074	285	10	0081	0	65535	65535	1	26.45	15984	-2185	-2185	8	96	71	4891	5108	134	134	65535	0	16500	00C0	9	4020	4012	3974	3978	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    11	11:01:33 AM	450	0074	285	10	0081	0	65535	65535	1	26.55	15963	-2182	-2183	8	96	71	4853	5108	133	133	65535	0	16500	00C0	9	4015	4006	3969	3973	0006	0000	0000	0000	0000	8044	0000	0004	13760	0000
    12	11:02:18 AM	495	0074	285	10	0081	0	65535	65535	1	26.65	15951	-2181	-2181	8	95	71	4834	5108	133	133	65535	1600	16500	00C0	9	4012	4003	3966	3970	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    13	11:03:03 AM	540	0074	285	10	0081	0	65535	65535	1	26.75	15931	-2178	-2179	8	94	70	4796	5108	132	132	65535	1600	16500	00C0	9	4007	3998	3961	3965	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    14	11:03:48 AM	585	0074	285	10	0081	0	65535	65535	1	26.75	15918	-2176	-2177	8	94	70	4776	5108	132	132	65535	1600	16500	00C0	9	4004	3994	3958	3962	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    15	11:04:33 AM	630	0074	285	10	0081	0	65535	65535	1	26.85	15895	-2174	-2174	8	93	69	4738	5108	131	131	65535	1600	16500	00C0	9	3997	3988	3953	3956	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    16	11:05:18 AM	675	0074	285	10	0081	0	65535	65535	1	26.85	15881	-2172	-2173	8	93	69	4719	5108	130	130	65535	1600	16500	00C0	9	3994	3984	3950	3953	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    17	11:06:03 AM	720	0074	285	10	0081	0	65535	65535	1	26.95	15869	-2171	-2171	8	93	69	4700	5108	130	130	65535	1600	16500	00C0	9	3991	3981	3947	3950	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    18	11:06:48 AM	765	0074	285	10	0081	0	65535	65535	1	27.05	15843	-2168	-2168	8	92	68	4662	5108	129	129	65535	1600	16500	00C0	9	3985	3974	3940	3943	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    19	11:07:33 AM	810	0074	285	10	0081	0	65535	65535	1	26.95	15831	-2165	-2166	8	91	68	4642	5108	129	129	65535	1600	16500	00C0	9	3982	3971	3938	3940	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    20	11:08:18 AM	855	0074	285	10	0081	0	65535	65535	1	27.05	15803	-2162	-2163	8	91	67	4604	5108	128	128	65535	1600	16500	00C0	9	3975	3964	3931	3933	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    21	11:09:03 AM	900	0074	285	10	0081	0	65535	65535	1	27.15	15789	-2160	-2161	8	90	67	4585	5108	127	127	65535	1600	16500	00C0	9	3971	3960	3928	3930	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    22	11:09:48 AM	945	0074	285	10	0081	0	65535	65535	1	27.25	15762	-2157	-2158	8	89	66	4546	5108	126	126	65535	1600	16500	00C0	9	3965	3954	3922	3923	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    23	11:10:33 AM	990	0074	285	10	0081	0	65535	65535	1	27.25	15748	-2155	-2156	8	89	66	4528	5108	126	126	65535	1600	16500	00C0	9	3961	3950	3918	3920	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    24	11:11:18 AM	1035	0074	285	10	0081	0	65535	65535	1	27.25	15736	-2153	-2154	8	89	66	4509	5108	126	126	65535	1600	16500	00C0	9	3958	3947	3914	3916	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    25	11:12:03 AM	1080	0074	285	10	0081	0	65535	65535	1	27.35	15705	-2149	-2150	8	88	65	4470	5108	125	125	65535	1600	16500	00C0	9	3950	3939	3907	3909	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    26	11:12:48 AM	1125	0074	285	10	0081	0	65535	65535	1	27.35	15693	-2148	-2149	8	88	65	4451	5108	124	124	65535	1600	16500	00C0	9	3947	3936	3904	3906	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    27	11:13:33 AM	1170	0074	285	10	0081	0	65535	65535	1	27.45	15665	-2144	-2145	8	87	64	4414	5108	124	123	65535	1600	16500	00C0	9	3940	3929	3897	3899	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    28	11:14:18 AM	1215	0074	285	10	0081	0	65535	65535	1	27.45	15649	-2142	-2143	8	87	64	4395	5108	123	123	65535	1600	16500	00C0	9	3936	3925	3893	3895	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    29	11:15:03 AM	1260	0074	285	10	0081	0	65535	65535	1	27.55	15636	-2141	-2141	8	86	64	4376	5108	123	123	65535	1600	16500	00C0	9	3933	3922	3890	3891	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    30	11:15:48 AM	1305	0074	285	10	0081	0	65535	65535	1	27.55	15608	-2137	-2138	8	85	63	4338	5108	122	122	65535	1600	16500	00C0	9	3927	3916	3883	3884	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    31	11:16:33 AM	1350	0074	285	10	0081	0	65535	65535	1	27.65	15596	-2135	-2136	8	85	63	4319	5108	121	121	65535	1600	16500	00C0	9	3923	3912	3880	3881	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    32	11:17:18 AM	1395	0074	285	10	0081	0	65535	65535	1	27.65	15568	-2132	-2133	8	84	63	4281	5108	120	120	65535	1600	16500	00C0	9	3916	3905	3873	3874	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    33	11:18:03 AM	1440	0074	285	10	0081	0	65535	65535	1	27.75	15556	-2130	-2131	8	84	62	4262	5108	120	120	65535	1600	16500	00C0	9	3913	3902	3870	3871	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    34	11:18:48 AM	1485	0074	285	10	0081	0	65535	65535	1	27.75	15543	-2128	-2129	8	84	62	4244	5108	120	120	65535	1600	16500	00C0	9	3910	3899	3866	3868	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    35	11:19:33 AM	1530	0074	285	10	0081	0	65535	65535	1	27.75	15519	-2125	-2126	8	83	61	4206	5108	119	119	65535	1600	16500	00C0	9	3903	3893	3860	3861	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    36	11:20:18 AM	1575	0074	285	10	0081	0	65535	65535	1	27.85	15505	-2123	-2124	8	82	61	4187	5108	118	118	65535	1600	16500	00C0	9	3900	3890	3857	3858	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    37	11:21:03 AM	1620	0074	285	10	0081	0	65535	65535	1	27.85	15481	-2120	-2121	8	82	61	4150	5108	117	117	65535	1600	16500	00C0	9	3894	3884	3851	3852	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    38	11:21:48 AM	1665	0074	285	10	0081	0	65535	65535	1	27.95	15471	-2118	-2119	8	81	60	4131	5108	117	117	65535	1600	16500	00C0	9	3892	3882	3848	3850	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    39	11:22:33 AM	1710	0074	285	10	0081	0	65535	65535	1	27.95	15445	-2116	-2116	8	81	60	4094	5108	116	116	65535	1600	16500	00C0	9	3885	3875	3841	3843	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    40	11:23:18 AM	1755	0074	285	10	0081	0	65535	65535	1	28.05	15436	-2114	-2114	8	80	60	4075	5108	116	116	65535	1600	16500	00C0	9	3883	3873	3839	3841	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    41	11:24:03 AM	1800	0074	285	10	0081	0	65535	65535	1	28.05	15425	-2112	-2113	8	80	59	4056	5108	115	115	65535	1600	16500	00C0	9	3880	3871	3836	3838	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    42	11:24:48 AM	1845	0074	285	10	0081	0	65535	65535	1	28.15	15404	-2110	-2110	8	79	59	4019	5108	114	114	65535	1600	16500	00C0	9	3875	3865	3831	3832	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    43	11:25:33 AM	1890	0074	285	10	0081	0	65535	65535	1	28.15	15392	-2107	-2109	8	79	58	4000	5108	114	114	65535	1600	16500	00C0	9	3872	3862	3828	3830	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    44	11:26:18 AM	1935	0074	285	10	0081	0	65535	65535	1	28.25	15372	-2105	-2106	8	78	58	3963	5108	113	113	65535	1600	16500	00C0	9	3867	3858	3823	3825	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    45	11:27:03 AM	1980	0074	285	10	0081	0	65535	65535	1	28.25	15361	-2104	-2104	8	78	58	3945	5108	112	112	65535	1600	16500	00C0	9	3864	3855	3820	3822	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    46	11:27:48 AM	2025	0074	285	10	0081	0	65535	65535	1	28.25	15350	-2103	-2103	8	77	57	3926	5108	112	112	65535	1600	16500	00C0	9	3861	3852	3817	3819	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    47	11:28:33 AM	2070	0074	285	10	0081	0	65535	65535	1	28.25	15332	-2100	-2101	8	77	57	3889	5108	111	111	65535	1600	16500	00C0	9	3857	3847	3813	3815	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    48	11:29:18 AM	2115	0074	285	10	0081	0	65535	65535	1	28.35	15320	-2099	-2099	8	76	57	3870	5108	111	111	65535	1600	16500	00C0	9	3854	3845	3809	3812	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    49	11:30:03 AM	2160	0074	285	10	0081	0	65535	65535	1	28.35	15301	-2096	-2097	8	76	56	3833	5108	110	110	65535	1600	16500	00C0	9	3850	3840	3805	3807	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    50	11:30:48 AM	2205	0074	285	10	0081	0	65535	65535	1	28.45	15293	-2095	-2095	8	75	56	3815	5108	109	109	65535	1600	16500	00C0	9	3847	3838	3803	3805	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    51	11:31:33 AM	2250	0074	285	10	0081	0	65535	65535	1	28.55	15273	-2092	-2093	8	74	55	3778	5108	108	108	65535	1600	16500	00C0	9	3842	3833	3798	3800	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    52	11:32:18 AM	2295	0074	285	10	0081	0	65535	65535	1	28.55	15264	-2091	-2092	8	74	55	3759	5108	108	108	65535	1600	16500	00C0	9	3840	3831	3796	3798	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    53	11:33:03 AM	2340	0074	285	10	0081	0	65535	65535	1	28.55	15253	-2090	-2090	8	74	55	3741	5108	107	107	65535	1600	16500	00C0	9	3837	3828	3793	3795	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    54	11:33:48 AM	2385	0074	285	10	0081	0	65535	65535	1	28.65	15234	-2088	-2088	8	73	54	3704	5108	106	106	65535	1600	16500	00C0	9	3832	3823	3788	3790	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    55	11:34:33 AM	2430	0074	285	10	0081	0	65535	65535	1	28.65	15227	-2086	-2087	8	73	54	3685	5108	106	106	65535	1600	16500	00C0	9	3831	3821	3786	3788	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    56	11:35:18 AM	2475	0074	285	10	0081	0	65535	65535	1	28.65	15208	-2083	-2084	8	72	53	3649	5108	105	105	65535	1600	16500	00C0	9	3826	3817	3782	3783	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    57	11:36:03 AM	2520	0074	285	10	0081	0	65535	65535	1	28.75	15198	-2082	-2083	8	72	53	3630	5108	105	105	65535	1600	16500	00C0	9	3824	3814	3779	3781	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    58	11:36:48 AM	2565	0074	285	10	0081	0	65535	65535	1	28.75	15189	-2081	-2082	8	71	53	3612	5108	104	104	65535	1600	16500	00C0	9	3821	3812	3777	3779	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    59	11:37:33 AM	2610	0074	285	10	0081	0	65535	65535	1	28.75	15170	-2079	-2079	8	70	52	3575	5108	103	103	65535	1600	16500	00C0	9	3816	3807	3773	3774	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    60	11:38:18 AM	2655	0074	285	10	0081	0	65535	65535	1	28.85	15161	-2077	-2078	8	70	52	3557	5108	103	103	65535	1600	16500	00C0	9	3814	3805	3770	3772	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    61	11:39:03 AM	2700	0074	285	10	0081	0	65535	65535	1	28.95	15142	-2075	-2076	8	69	52	3520	5108	102	102	65535	1600	16500	00C0	9	3809	3800	3765	3767	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    62	11:39:48 AM	2745	0074	285	10	0081	0	65535	65535	1	29.15	15133	-2074	-2075	8	69	51	3502	5108	101	101	65535	1600	16500	00C0	9	3807	3798	3763	3765	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    63	11:40:33 AM	2790	0074	285	10	0081	0	65535	65535	1	29.35	15113	-2072	-2073	8	68	51	3466	5108	100	100	65535	1600	16500	00C0	9	3802	3793	3758	3760	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    64	11:41:18 AM	2835	0074	285	10	0081	0	65535	65535	1	29.45	15102	-2071	-2071	8	68	50	3447	5108	100	100	65535	1600	16500	00C0	9	3799	3790	3756	3757	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    65	11:42:03 AM	2880	0074	285	10	0081	0	65535	65535	1	29.55	15094	-2069	-2070	8	68	50	3429	5108	99	99	65535	1600	16500	00C0	9	3797	3788	3754	3755	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    66	11:42:48 AM	2925	0074	285	10	0081	0	65535	65535	1	29.65	15074	-2067	-2068	8	67	50	3393	5108	98	98	65535	1600	16500	00C0	9	3792	3783	3749	3750	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    67	11:43:33 AM	2970	0074	285	10	0081	0	65535	65535	1	29.85	15063	-2066	-2066	8	67	49	3374	5108	98	98	65535	1600	16500	00C0	9	3789	3781	3747	3747	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    68	11:44:18 AM	3015	0074	285	10	0081	0	65535	65535	1	29.95	15043	-2064	-2064	8	66	49	3338	5108	97	97	65535	1600	16500	00C0	9	3784	3775	3742	3742	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    69	11:45:03 AM	3060	0074	285	10	0081	0	65535	65535	1	30.05	15034	-2062	-2063	8	65	49	3319	5108	97	97	65535	1600	16500	00C0	9	3781	3773	3739	3740	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    70	11:45:48 AM	3105	0074	285	10	0081	0	65535	65535	1	30.05	15022	-2060	-2061	8	65	48	3302	5108	96	96	65535	1600	16500	00C0	9	3779	3769	3737	3737	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    71	11:46:33 AM	3150	0074	285	10	0081	0	65535	65535	1	30.15	15001	-2058	-2058	8	64	48	3265	5108	95	95	65535	1600	16500	00C0	9	3774	3764	3731	3732	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    72	11:47:18 AM	3195	0074	285	10	0081	0	65535	65535	1	30.15	14992	-2057	-2057	8	64	48	3247	5108	95	95	65535	1600	16500	00C0	9	3771	3761	3729	3730	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    73	11:48:03 AM	3240	0074	285	10	0081	0	65535	65535	1	30.25	14970	-2054	-2054	8	63	47	3211	5108	94	94	65535	1600	16500	00C0	9	3766	3756	3724	3724	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    74	11:48:48 AM	3285	0074	285	10	0081	0	65535	65535	1	30.25	14960	-2052	-2053	8	63	47	3193	5108	93	93	65535	1600	16500	00C0	9	3763	3754	3721	3722	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    75	11:49:33 AM	3330	0074	285	10	0081	0	65535	65535	1	30.35	14939	-2050	-2050	8	62	46	3157	5108	92	92	65535	1600	16500	00C0	9	3758	3748	3716	3717	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    76	11:50:18 AM	3375	0074	285	10	0081	0	65535	65535	1	30.35	14929	-2048	-2049	8	62	46	3139	5108	92	92	65535	1600	16500	00C0	9	3755	3746	3714	3714	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    77	11:51:03 AM	3420	0074	285	10	0081	0	65535	65535	1	30.35	14919	-2047	-2047	8	62	46	3121	5108	91	91	65535	1600	16500	00C0	9	3753	3743	3711	3712	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    78	11:51:48 AM	3465	0074	285	10	0081	0	65535	65535	1	30.35	14897	-2044	-2044	8	61	45	3085	5108	91	91	65535	1600	16500	00C0	9	3747	3737	3706	3706	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    79	11:52:33 AM	3510	0074	285	10	0081	0	65535	65535	1	30.35	14884	-2042	-2043	8	61	45	3067	5108	90	90	65535	1600	16500	00C0	9	3744	3734	3703	3703	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    80	11:53:18 AM	3555	0074	285	10	0081	0	65535	65535	1	30.35	14865	-2040	-2040	8	60	44	3031	5108	89	89	65535	1600	16500	00C0	9	3739	3729	3698	3698	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    81	11:54:03 AM	3600	0074	285	10	0081	0	65535	65535	1	30.35	14854	-2038	-2039	8	59	44	3013	5108	89	89	65535	1600	16500	00C0	9	3736	3727	3695	3696	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    82	11:54:48 AM	3645	0074	285	10	0081	0	65535	65535	1	30.35	14844	-2036	-2037	8	59	44	2995	5108	88	88	65535	1600	16500	00C0	9	3734	3724	3693	3693	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    83	11:55:33 AM	3690	0074	285	10	0081	0	65535	65535	1	30.35	14822	-2033	-2034	8	58	43	2959	5108	87	87	65535	1600	16500	00C0	9	3728	3719	3688	3687	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    84	11:56:18 AM	3735	0074	285	10	0081	0	65535	65535	1	30.25	14811	-2031	-2032	8	58	43	2941	5108	87	87	65535	1600	16500	00C0	9	3725	3716	3685	3685	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    85	11:57:03 AM	3780	0074	285	10	0081	0	65535	65535	1	30.25	14789	-2028	-2029	8	57	43	2906	5108	86	86	65535	1600	16500	00C0	9	3720	3710	3680	3679	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    86	11:57:48 AM	3825	0074	285	10	0081	0	65535	65535	1	30.25	14778	-2027	-2028	8	57	42	2887	5108	85	85	65535	1600	16500	00C0	9	3717	3708	3677	3676	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    87	11:58:33 AM	3870	0074	285	10	0081	0	65535	65535	1	30.25	14757	-2023	-2024	8	56	42	2851	5108	85	85	65535	1600	16500	00C0	9	3712	3702	3671	3671	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    88	11:59:18 AM	3915	0074	285	10	0081	0	65535	65535	1	30.25	14745	-2022	-2023	8	56	42	2834	5108	84	84	65535	1600	16500	00C0	9	3709	3699	3669	3668	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    89	12:00:03 PM	3960	0074	285	10	0081	0	65535	65535	1	30.15	14735	-2021	-2021	8	56	41	2816	5108	84	84	65535	1600	16500	00C0	9	3706	3697	3666	3666	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    90	12:00:48 PM	4005	0074	285	10	0081	0	65535	65535	1	30.15	14712	-2018	-2018	8	55	41	2780	5108	83	83	65535	1600	16500	00C0	9	3700	3691	3661	3660	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    91	12:01:33 PM	4050	0074	285	10	0081	0	65535	65535	1	30.15	14701	-2016	-2017	8	55	41	2763	5108	82	82	65535	1600	16500	00C0	9	3697	3688	3658	3657	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    92	12:02:18 PM	4095	0074	285	10	0081	0	65535	65535	1	30.15	14680	-2012	-2013	8	54	40	2727	5108	81	81	65535	1600	16500	00C0	9	3692	3683	3653	3652	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    93	12:03:03 PM	4140	0074	285	10	0081	0	65535	65535	1	30.15	14668	-2011	-2012	8	54	40	2709	5108	81	81	65535	1600	16500	00C0	9	3689	3680	3650	3649	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    94	12:03:48 PM	4185	0074	285	10	0081	0	65535	65535	1	30.05	14656	-2010	-2010	8	53	40	2692	5108	80	80	65535	1600	16500	00C0	9	3686	3677	3647	3646	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    95	12:04:33 PM	4230	0074	285	10	0081	0	65535	65535	1	30.05	14633	-2007	-2007	8	52	39	2656	5108	79	79	65535	1600	16500	00C0	9	3680	3671	3642	3640	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    96	12:05:18 PM	4275	0074	285	10	0081	0	65535	65535	1	30.05	14624	-2005	-2006	8	52	39	2638	5108	79	79	65535	1600	16500	00C0	9	3678	3669	3639	3638	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    97	12:06:03 PM	4320	0074	285	10	0081	0	65535	65535	1	29.95	14601	-2001	-2003	8	51	38	2603	5108	78	78	65535	1600	16500	00C0	9	3673	3664	3633	3633	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    98	12:06:48 PM	4365	0074	285	10	0081	0	65535	65535	1	29.85	14592	-2000	-2001	8	51	38	2585	5108	78	78	65535	1600	16500	00C0	9	3670	3661	3631	3630	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    99	12:07:33 PM	4410	0074	285	10	0081	0	65535	65535	1	29.85	14571	-1997	-1998	8	50	37	2550	5108	77	77	65535	1600	16500	00C0	9	3665	3656	3625	3625	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    100	12:08:18 PM	4455	0074	285	10	0081	0	65535	65535	1	29.85	14560	-1996	-1996	8	50	37	2533	5108	76	76	65535	1600	16500	00C0	9	3662	3653	3623	3622	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    101	12:09:03 PM	4500	0074	285	10	0081	0	65535	65535	1	29.85	14549	-1994	-1994	8	50	37	2515	5108	76	76	65535	1600	16500	00C0	9	3659	3651	3620	3619	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    102	12:09:48 PM	4545	0074	285	10	0081	0	65535	65535	1	29.85	14527	-1991	-1992	8	49	36	2480	5108	75	75	65535	1600	16500	00C0	9	3654	3645	3614	3614	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    103	12:10:33 PM	4590	0074	285	10	0081	0	65535	65535	1	29.85	14517	-1989	-1990	8	49	36	2462	5108	74	74	65535	1600	16500	00C0	9	3651	3643	3612	3611	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    104	12:11:18 PM	4635	0074	285	10	0081	0	65535	65535	1	29.95	14499	-1987	-1987	8	48	36	2427	5108	73	73	65535	1600	16500	00C0	9	3646	3638	3607	3607	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    105	12:12:03 PM	4680	0074	285	10	0081	0	65535	65535	1	29.95	14487	-1985	-1986	8	48	35	2410	5108	73	73	65535	1600	16500	00C0	9	3643	3635	3604	3604	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    106	12:12:48 PM	4725	0074	285	10	0081	0	65535	65535	1	29.95	14478	-1984	-1984	8	47	35	2392	5108	72	72	65535	1600	16500	00C0	9	3641	3633	3602	3602	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    107	12:13:33 PM	4770	0074	285	10	0081	0	65535	65535	1	29.75	14458	-1981	-1982	8	47	35	2357	5108	71	71	65535	1600	16500	00C0	9	3636	3628	3597	3597	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    108	12:14:18 PM	4815	0074	285	10	0081	0	65535	65535	1	29.65	14449	-1980	-1980	8	46	34	2339	5108	71	71	65535	1600	16500	00C0	9	3634	3626	3595	3594	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    109	12:15:03 PM	4860	0074	285	10	0081	0	65535	65535	1	29.55	14428	-1977	-1977	8	46	34	2305	5108	70	70	65535	1600	16500	00C0	9	3629	3620	3589	3589	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    110	12:15:48 PM	4905	0074	285	10	0081	0	65535	65535	1	29.45	14420	-1975	-1976	8	45	34	2287	5108	69	69	65535	1600	16500	00C0	9	3627	3619	3587	3587	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    111	12:16:33 PM	4950	0074	285	10	0081	0	65535	65535	1	29.25	14400	-1973	-1973	8	45	33	2252	5108	68	68	65535	1600	16500	00C0	9	3622	3613	3582	3582	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    112	12:17:18 PM	4995	0074	285	10	0081	0	65535	65535	1	29.15	14390	-1971	-1972	8	44	33	2235	5108	68	68	65535	1600	16500	00C0	9	3619	3611	3580	3580	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    113	12:18:03 PM	5040	0074	285	10	0081	0	65535	65535	1	29.05	14383	-1970	-1970	8	44	33	2217	5108	68	68	65535	1600	16500	00C0	9	3618	3609	3578	3578	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    114	12:18:48 PM	5085	0074	285	10	0081	0	65535	65535	1	29.05	14365	-1967	-1968	8	43	32	2183	5108	67	67	65535	1600	16500	00C0	9	3613	3605	3574	3573	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    115	12:19:33 PM	5130	0074	285	10	0081	0	65535	65535	1	28.95	14355	-1966	-1967	8	43	32	2165	5108	66	66	65535	1600	16500	00C0	9	3611	3603	3571	3571	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    116	12:20:18 PM	5175	0074	285	10	0081	0	65535	65535	1	28.95	14336	-1963	-1964	8	42	31	2130	5108	65	65	65535	1600	16500	00C0	9	3606	3598	3566	3566	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    117	12:21:03 PM	5220	0074	285	10	0081	0	65535	65535	1	28.95	14329	-1962	-1962	8	42	31	2113	5108	65	65	65535	1600	16500	00C0	9	3603	3596	3564	3564	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    118	12:21:48 PM	5265	0074	285	10	0081	0	65535	65535	1	28.95	14319	-1961	-1961	8	42	31	2096	5108	64	64	65535	1600	16500	00C0	9	3602	3594	3562	3562	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    119	12:22:33 PM	5310	0074	285	10	0081	0	65535	65535	1	29.05	14303	-1959	-1959	8	41	30	2061	5108	63	63	65535	1600	16500	00C0	9	3598	3590	3558	3558	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    120	12:23:18 PM	5355	0074	285	10	0081	0	65535	65535	1	29.15	14293	-1958	-1958	8	41	30	2044	5108	63	63	65535	1600	16500	00C0	9	3595	3587	3555	3556	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    121	12:24:03 PM	5400	0074	285	10	0081	0	65535	65535	1	29.35	14276	-1955	-1956	8	40	30	2009	5108	62	62	65535	1600	16500	00C0	9	3591	3583	3551	3551	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    122	12:24:49 PM	5446	0074	285	10	0081	0	65535	65535	1	29.45	14269	-1953	-1954	8	39	29	1992	5108	61	61	65535	1600	16500	00C0	9	3589	3581	3550	3549	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    123	12:25:34 PM	5491	0074	285	10	0081	0	65535	65535	1	29.55	14253	-1952	-1952	8	39	29	1957	5108	60	60	65535	1600	16500	00C0	9	3585	3577	3545	3545	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    124	12:26:19 PM	5536	0074	285	10	0081	0	65535	65535	1	29.55	14243	-1951	-1951	8	38	29	1940	5108	60	60	65535	1600	16500	00C0	9	3582	3575	3543	3543	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    125	12:27:04 PM	5581	0074	285	10	0081	0	65535	65535	1	29.55	14236	-1950	-1950	8	38	28	1923	5108	59	59	65535	1600	16500	00C0	9	3581	3573	3541	3541	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    126	12:27:49 PM	5626	0074	285	10	0081	0	65535	65535	1	29.65	14220	-1948	-1948	8	37	28	1889	5108	58	58	65535	1600	16500	00C0	9	3576	3569	3537	3537	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    127	12:28:34 PM	5671	0074	285	10	0081	0	65535	65535	1	29.75	14211	-1947	-1947	8	37	28	1871	5108	58	58	65535	1600	16500	00C0	9	3574	3567	3535	3535	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    128	12:29:19 PM	5716	0074	285	10	0081	0	65535	65535	1	29.85	14198	-1945	-1945	8	36	27	1837	5108	57	57	65535	1600	16500	00C0	9	3571	3563	3532	3531	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    129	12:30:04 PM	5761	0074	285	10	0081	0	65535	65535	1	29.85	14189	-1944	-1944	8	36	27	1820	5108	56	56	65535	1600	16500	00C0	9	3569	3561	3530	3529	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    130	12:30:49 PM	5806	0074	285	10	0081	0	65535	65535	1	29.85	14180	-1942	-1942	8	36	27	1803	5108	56	56	65535	1600	16500	00C0	9	3566	3559	3528	3527	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    131	12:31:34 PM	5851	0074	285	10	0081	0	65535	65535	1	29.95	14164	-1940	-1940	8	35	26	1769	5108	55	55	65535	1600	16500	00C0	9	3562	3554	3524	3523	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    132	12:32:19 PM	5896	0074	285	10	0081	0	65535	65535	1	30.05	14155	-1939	-1939	8	35	26	1751	5108	54	54	65535	1600	16500	00C0	9	3560	3552	3522	3521	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    133	12:33:04 PM	5941	0074	285	10	0081	0	65535	65535	1	30.05	14139	-1937	-1937	8	34	25	1717	5108	53	53	65535	1600	16500	00C0	9	3556	3548	3518	3517	0006	0000	0000	0000	0000	8044	0400	0004	13760	0000
    134	12:33:49 PM	5986	0074	285	10	0081	0	65535	65535	1	30.05	14131	-1936	-1936	8	34	25	1700	5108	53	53	65535	1600	16500	00C0	9	3554	3546	3516	3515	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    135	12:34:34 PM	6031	0074	285	10	0081	0	65535	65535	1	30.15	14123	-1935	-1935	8	33	25	1683	5108	52	52	65535	1600	16500	00C0	9	3552	3544	3514	3513	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    136	12:35:19 PM	6076	0074	285	10	0081	0	65535	65535	1	30.25	14107	-1933	-1933	8	33	24	1649	5108	51	51	65535	1600	16500	00C0	9	3548	3540	3510	3509	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    137	12:36:04 PM	6121	0074	285	10	0081	0	65535	65535	1	30.25	14099	-1932	-1932	8	32	24	1632	5108	51	51	65535	1600	16500	00C0	9	3546	3538	3508	3507	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    138	12:36:49 PM	6166	0074	285	10	0081	0	65535	65535	1	30.25	14081	-1929	-1930	8	32	24	1598	5108	50	50	65535	1600	16500	00C0	9	3541	3533	3504	3503	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    139	12:37:34 PM	6211	0074	285	10	0081	0	65535	65535	1	30.35	14074	-1928	-1929	8	31	23	1581	5108	49	49	65535	1600	16500	00C0	9	3540	3531	3502	3501	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    140	12:38:19 PM	6256	0074	285	10	0081	0	65535	65535	1	30.35	14058	-1926	-1927	8	31	23	1547	5108	48	48	65535	1600	16500	00C0	9	3536	3527	3498	3497	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    141	12:39:04 PM	6301	0074	285	10	0081	0	65535	65535	1	30.35	14049	-1925	-1926	8	30	23	1530	5108	48	48	65535	1600	16500	00C0	9	3533	3525	3496	3495	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    142	12:39:49 PM	6346	0074	285	10	0081	0	65535	65535	1	30.45	14041	-1924	-1925	8	30	22	1513	5108	47	47	65535	1600	16500	00C0	9	3531	3523	3494	3493	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    143	12:40:34 PM	6391	0074	285	10	0081	0	65535	65535	1	30.45	14021	-1922	-1922	8	29	22	1479	5108	46	46	65535	1600	16500	00C0	9	3526	3518	3489	3489	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    144	12:41:19 PM	6436	0074	285	10	0081	0	65535	65535	1	30.55	14014	-1921	-1921	8	29	22	1462	5108	46	46	65535	1600	16500	00C0	9	3524	3516	3488	3486	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    145	12:42:04 PM	6481	0074	285	10	0081	0	65535	65535	1	30.55	13997	-1919	-1919	8	28	21	1428	5108	45	45	65535	1600	16500	00C0	9	3520	3512	3483	3482	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    146	12:42:49 PM	6526	0074	285	10	0081	0	65535	65535	1	30.65	13989	-1917	-1918	8	28	21	1411	5108	44	44	65535	1600	16500	00C0	9	3518	3510	3481	3480	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    147	12:43:34 PM	6571	0074	285	10	0081	0	65535	65535	1	30.65	13970	-1915	-1915	8	27	20	1378	5108	43	43	65535	1600	16500	00C0	9	3513	3505	3477	3475	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    148	12:44:19 PM	6616	0074	285	10	0081	0	65535	65535	1	30.65	13962	-1914	-1914	8	27	20	1361	5108	43	43	65535	1600	16500	00C0	9	3511	3503	3475	3473	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    149	12:45:04 PM	6661	0074	285	10	0081	0	65535	65535	1	30.75	13953	-1913	-1913	8	27	20	1344	5108	42	42	65535	1600	16500	00C0	9	3508	3500	3473	3471	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    150	12:45:49 PM	6706	0074	285	10	0081	0	65535	65535	1	30.75	13934	-1910	-1911	8	26	19	1310	5108	41	41	65535	1600	16500	00C0	9	3504	3496	3468	3466	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    151	12:46:34 PM	6751	0074	285	10	0081	0	65535	65535	1	30.85	13921	-1909	-1909	8	26	19	1293	5108	41	41	65535	1600	16500	00C0	9	3500	3493	3465	3463	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    152	12:47:19 PM	6796	0074	285	10	0081	0	65535	65535	1	30.75	13904	-1906	-1906	8	25	19	1260	5108	40	40	65535	1600	16500	00C0	9	3496	3488	3461	3459	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    153	12:48:04 PM	6841	0074	285	10	0081	0	65535	65535	1	30.85	13895	-1905	-1905	8	25	19	1243	5108	39	39	65535	1600	16500	00C0	9	3493	3486	3458	3456	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    154	12:48:49 PM	6886	0074	285	10	0081	0	65535	65535	1	30.85	13884	-1903	-1904	8	25	18	1226	5108	39	39	65535	1600	16500	00C0	9	3491	3483	3456	3454	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    155	12:49:34 PM	6931	0074	285	10	0081	0	65535	65535	1	30.95	13862	-1901	-1901	8	24	18	1192	5108	38	38	65535	1600	16500	00C0	9	3485	3477	3451	3449	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    156	12:50:19 PM	6976	0074	285	10	0081	0	65535	65535	1	30.95	13852	-1899	-1900	8	24	18	1176	5108	37	37	65535	1600	16500	00C0	9	3482	3475	3448	3446	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    157	12:51:04 PM	7021	0074	285	10	0081	0	65535	65535	1	30.95	13830	-1896	-1897	8	23	17	1142	5108	36	36	65535	1600	16500	00C0	9	3477	3469	3443	3441	0006	0000	0000	0000	0000	8044	0200	0008	13760	0000
    158	12:51:49 PM	7066	0074	285	10	0081	0	65535	65535	1	31.15	13819	-1894	-1895	8	8	5	344	4852	11	11	65535	1600	16500	00C0	9	3474	3466	3441	3438	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    159	12:52:34 PM	7111	0074	285	10	0081	0	65535	65535	1	31.15	13807	-1893	-1894	8	7	5	328	4852	10	10	65535	1600	16500	00C0	9	3471	3463	3438	3435	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    160	12:53:19 PM	7156	0074	285	10	0081	0	65535	65535	1	31.35	13783	-1889	-1891	8	7	5	294	4852	9	9	65535	1600	16500	01C0	9	3465	3457	3432	3429	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    161	12:54:04 PM	7201	0074	285	10	0081	0	65535	65535	1	31.45	13771	-1889	-1889	8	6	5	278	4852	9	9	65535	1600	16500	0BC0	9	3462	3454	3429	3426	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    162	12:54:49 PM	7246	0074	285	10	0081	0	65535	65535	1	31.55	13747	-1886	-1886	8	6	4	245	4852	8	8	65535	1600	16500	0BC0	9	3455	3448	3424	3420	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    163	12:55:34 PM	7291	0074	285	10	0081	0	65535	65535	1	31.65	13735	-1884	-1885	8	5	4	228	4852	7	7	65535	1600	16500	0BC0	9	3452	3445	3421	3417	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    164	12:56:19 PM	7336	0074	285	10	0081	0	65535	65535	1	31.75	13710	-1881	-1882	8	4	3	194	4852	6	6	65535	1600	16500	0BC0	9	3445	3439	3415	3411	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    165	12:57:04 PM	7381	0074	285	10	0081	0	65535	65535	1	31.85	13698	-1880	-1880	8	4	3	178	4852	6	6	65535	1600	16500	0BC0	9	3443	3436	3411	3408	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    166	12:57:49 PM	7426	0074	285	10	0081	0	65535	65535	1	31.95	13688	-1878	-1879	8	4	3	161	4852	5	5	65535	1600	16500	0BC0	9	3440	3434	3409	3405	0006	0000	0000	0000	0000	8048	0200	0008	13600	0000
    167	12:58:34 PM	7471	0074	285	10	0081	0	65535	65535	1	32.05	13665	-1875	-1876	8	3	2	129	4852	4	4	65535	1600	16500	0BC0	9	3435	3428	3403	3399	0006	0000	0000	0000	0000	8048	0200	0008	13560	0000
    168	12:59:19 PM	7516	0074	285	10	0081	0	65535	65535	1	32.05	13655	-1874	-1875	8	3	2	112	4852	4	4	65535	1600	16500	0BC0	9	3432	3426	3400	3397	0006	0000	0000	0000	0000	8048	0200	0008	13560	0000
    169	1:00:04 PM	7561	0074	285	10	0081	0	65535	65535	1	32.15	13635	-1871	-1872	8	2	2	79	4852	3	3	65535	1600	16500	0BD0	9	3428	3422	3394	3392	0006	0000	0000	0000	0000	8048	0200	0008	13560	0000
    170	1:00:49 PM	7606	0074	285	10	0081	0	65535	65535	0	32.25	13625	-1870	-1871	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3425	3419	3392	3389	0006	0000	0000	0000	0000	8048	0200	0008	13560	0000
    171	1:01:34 PM	7651	0074	285	10	0081	0	65535	65535	0	32.25	13615	-1869	-1869	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3423	3416	3389	3387	0006	0000	0000	0000	0000	8048	0200	0008	13560	0000
    172	1:02:19 PM	7696	0074	285	10	0081	0	65535	65535	0	32.25	13595	-1866	-1867	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3418	3411	3384	3382	0006	0000	0000	0000	0000	8048	0200	0008	13560	0000
    173	1:03:04 PM	7741	0074	285	10	0081	0	65535	65535	0	32.25	13585	-1865	-1866	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3415	3408	3382	3379	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    174	1:03:49 PM	7786	0074	285	10	0081	0	65535	65535	0	32.25	13563	-1863	-1863	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3409	3403	3377	3374	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    175	1:04:34 PM	7831	0074	285	10	0081	0	65535	65535	0	32.25	13555	-1861	-1862	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3407	3401	3374	3372	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    176	1:05:19 PM	7876	0074	285	10	0081	0	65535	65535	0	32.35	13532	-1857	-1858	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3401	3395	3369	3366	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    177	1:06:04 PM	7921	0074	285	10	0081	0	65535	65535	0	32.35	13521	-1856	-1857	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3398	3392	3367	3364	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    178	1:06:49 PM	7966	0074	285	10	0081	0	65535	65535	0	32.35	13509	-1855	-1855	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3395	3389	3364	3361	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    179	1:07:34 PM	8011	0074	285	10	0081	0	65535	65535	0	32.45	13485	-1851	-1852	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3389	3383	3359	3355	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    180	1:08:19 PM	8056	0074	285	10	0081	0	65535	65535	0	32.45	13472	-1850	-1851	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3385	3379	3356	3352	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    181	1:09:04 PM	8101	0074	285	10	0081	0	65535	65535	0	32.45	13447	-1846	-1847	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3379	3372	3350	3345	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    182	1:09:49 PM	8146	0074	285	10	0081	0	65535	65535	0	32.45	13433	-1844	-1845	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3375	3368	3346	3342	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    183	1:10:34 PM	8191	0074	285	10	0081	0	65535	65535	0	32.45	13417	-1843	-1843	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3371	3365	3343	3338	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    184	1:11:19 PM	8236	0074	285	10	0081	0	65535	65535	0	32.45	13388	-1839	-1840	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3363	3356	3337	3331	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    185	1:12:04 PM	8281	0074	285	10	0081	0	65535	65535	0	32.45	13370	-1836	-1837	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3358	3352	3333	3327	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    186	1:12:49 PM	8326	0074	285	10	0081	0	65535	65535	0	32.55	13336	-1831	-1832	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3348	3342	3326	3318	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    187	1:13:34 PM	8371	0074	285	10	0081	0	65535	65535	0	32.55	13315	-1829	-1830	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3343	3336	3321	3314	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    188	1:14:19 PM	8416	0074	285	10	0081	0	65535	65535	0	32.55	13268	-1822	-1824	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3331	3323	3312	3303	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    189	1:15:04 PM	8461	0074	285	10	0081	0	65535	65535	0	32.65	13242	-1819	-1820	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3323	3315	3307	3297	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    190	1:15:49 PM	8506	0074	285	10	0081	0	65535	65535	0	32.65	13214	-1815	-1817	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3315	3307	3302	3290	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    191	1:16:34 PM	8551	0074	285	10	0081	0	65535	65535	0	32.75	13153	-1806	-1808	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3298	3290	3290	3275	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    192	1:17:19 PM	8596	0074	285	10	0081	0	65535	65535	0	32.75	13119	-1803	-1804	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3289	3281	3282	3267	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    193	1:18:04 PM	8641	0074	285	10	0081	0	65535	65535	0	32.85	13054	-1794	-1795	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3273	3265	3266	3250	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    194	1:18:49 PM	8686	0074	285	10	0081	0	65535	65535	0	32.85	13024	-1789	-1791	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3266	3258	3258	3242	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    195	1:19:34 PM	8731	0074	285	10	0081	0	65535	65535	0	32.85	12994	-1785	-1787	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3259	3252	3249	3234	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    196	1:20:19 PM	8776	0074	285	10	0081	0	65535	65535	0	32.85	12939	-1777	-1779	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3246	3239	3234	3220	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    197	1:21:04 PM	8821	0074	285	10	0081	0	65535	65535	0	32.85	12912	-1774	-1776	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3239	3233	3227	3213	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    198	1:21:49 PM	8866	0074	285	10	0081	0	65535	65535	0	32.85	12862	-1767	-1769	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3227	3220	3214	3201	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    199	1:22:34 PM	8911	0074	285	10	0081	0	65535	65535	0	32.85	12835	-1763	-1765	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3220	3213	3208	3194	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    200	1:23:19 PM	8956	0074	285	10	0081	0	65535	65535	0	32.85	12782	-1756	-1758	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3206	3200	3195	3181	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    201	1:24:04 PM	9001	0074	285	10	0081	0	65535	65535	0	32.85	12782	-1756	-1758	8	0	0	0	4852	0	0	65535	1600	16500	0BD0	9	3206	3200	3195	3181	0004	0000	0080	0000	0000	8068	0200	0008	13560	0000
    202	1:24:49 PM	9046	0074	285	10	0081	0	65535	65535	1	32.75	13076	4	-6	8	0	0	0	4852	65535	0	65535	1600	16500	0BD0	9	3278	3272	3266	3262	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    203	1:25:34 PM	9091	0074	285	10	0081	0	65535	65535	1	32.65	13096	4	3	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3283	3276	3270	3267	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    204	1:26:19 PM	9136	0074	285	10	0081	0	65535	65535	1	32.55	13109	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3286	3280	3273	3270	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    205	1:27:04 PM	9181	0074	285	10	0081	0	65535	65535	1	32.45	13127	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3291	3285	3278	3275	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    206	1:27:49 PM	9226	0074	285	10	0081	0	65535	65535	1	32.45	13134	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3293	3286	3279	3276	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    207	1:28:34 PM	9271	0074	285	10	0081	0	65535	65535	1	32.25	13145	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3296	3289	3281	3279	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    208	1:29:19 PM	9316	0074	285	10	0081	0	65535	65535	1	32.25	13149	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3297	3290	3283	3280	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    209	1:30:04 PM	9361	0074	285	10	0081	0	65535	65535	1	31.95	13157	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3299	3292	3284	3282	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    210	1:30:49 PM	9406	0074	285	10	0081	0	65535	65535	1	31.85	13161	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3300	3293	3285	3283	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    211	1:31:34 PM	9451	0074	285	10	0081	0	65535	65535	1	31.75	13164	5	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3301	3294	3286	3284	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    212	1:32:19 PM	9496	0074	285	10	0081	0	65535	65535	1	31.65	13169	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3302	3295	3287	3285	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    213	1:33:04 PM	9541	0074	285	10	0081	0	65535	65535	1	31.55	13173	5	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3303	3296	3288	3286	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    214	1:33:49 PM	9586	0074	285	10	0081	0	65535	65535	1	31.45	13177	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3304	3297	3289	3287	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    215	1:34:34 PM	9631	0074	285	10	0081	0	65535	65535	1	31.35	13179	5	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3304	3298	3290	3287	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    216	1:35:19 PM	9676	0074	285	10	0081	0	65535	65535	1	31.25	13181	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3305	3298	3290	3288	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    217	1:36:04 PM	9721	0074	285	10	0081	0	65535	65535	1	31.15	13184	5	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3305	3299	3291	3289	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    218	1:36:49 PM	9766	0074	285	10	0081	0	65535	65535	1	31.15	13187	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3306	3300	3291	3289	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    219	1:37:34 PM	9811	0074	285	10	0081	0	65535	65535	1	30.95	13191	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3307	3301	3292	3290	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    220	1:38:19 PM	9856	0074	285	10	0081	0	65535	65535	1	30.85	13191	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3308	3301	3292	3291	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    221	1:39:04 PM	9901	0074	285	10	0081	0	65535	65535	1	30.85	13195	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3309	3302	3293	3292	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    222	1:39:49 PM	9946	0074	285	10	0081	0	65535	65535	1	30.75	13196	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3309	3302	3293	3292	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    223	1:40:34 PM	9991	0074	285	10	0081	0	65535	65535	1	30.75	13197	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3309	3302	3294	3292	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    224	1:41:19 PM	10036	0074	285	10	0081	0	65535	65535	1	30.65	13199	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3309	3303	3294	3293	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    225	1:42:04 PM	10081	0074	285	10	0081	0	65535	65535	1	30.55	13200	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3310	3303	3294	3293	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    226	1:42:49 PM	10126	0074	285	10	0081	0	65535	65535	1	30.45	13204	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3311	3304	3295	3294	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    227	1:43:34 PM	10171	0074	285	10	0081	0	65535	65535	1	30.35	13204	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3311	3304	3295	3294	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    228	1:44:19 PM	10216	0074	285	10	0081	0	65535	65535	1	30.35	13206	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3312	3305	3296	3294	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    229	1:45:04 PM	10261	0074	285	10	0081	0	65535	65535	1	30.25	13208	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3312	3305	3296	3295	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    230	1:45:49 PM	10306	0074	285	10	0081	0	65535	65535	1	30.25	13209	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3312	3306	3296	3295	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    231	1:46:34 PM	10351	0074	285	10	0081	0	65535	65535	1	30.15	13210	4	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3312	3306	3296	3296	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    232	1:47:19 PM	10396	0074	285	10	0081	0	65535	65535	1	30.05	13212	5	4	8	0	0	0	4852	65535	65535	65535	1600	16500	0AD0	9	3313	3306	3297	3296	0004	0000	0080	0000	0000	8060	0200	0008	13560	0000
    

    After discharge approx. 20 min is Battery REST Period data. ( LOAD Disconnected )

  • Hello Bhupendra,

    I see that this same topic is being discussed in another thread where there is a lot more information.

    https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1126457/bq3050-battery-discharge-voltage-up-after-rest-period/4209624

    Let's close this thread and keep the discussion going on the other thread.

  • Yes , Shirsh

    But the thing is : Seems no solution  and ending up with board may have Fault.

    Anyway, I m closing this and will separate thread.

    Thanks,