This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: Need firmware file for UCD90160A

Part Number: UCD90160A
Other Parts Discussed in Thread: UCD90SEQ64EVM-650, UCD90160

Hi,

I need to re-program the UCD90160 into the UCD901610A. I have the UCD90SEQ64EVM-650 board and the UCD90160 parts.

The UCD90xxx Firmware Upgrade Guide provides this guidance: (after installing the FDPD) download the new firmware into the device using the Firmware Download Tool to upgrade the device so that the script file can be exported later. Please consult TI to get the desired firmware file.

Herein, I am consulting TI (I hope) and asking for this firmware file or link to it if such link exists.

Same question was asked by another TI Forum member 4+years ago but was left unanswered.

Thank you,

GK