Hi Experts,
My customer is asking about the peak I_DS. There is a chance that a I_DS flows over 231A which violates abl max of this FET when a failure occurs. Customer wants to know if this pulse peak current is acceptable.
Below is the detail condition.
V_DS : 48V
I_DS(continuous) : 2.5A
H bridge for motor (inductive load) so four FET are used in a system.
Pulse width : 2us => This is the delay when system detects an over current then shut off a FET. Once a failure is detected, the system does not continue to run so only a single pulse is applied.
I_DS at short : possbile to flow over 231A, not sure how much the curernt flow.
Is this acceptable?
Regards,
Uchikoshi