Other Parts Discussed in Thread: TIDA-01505, PMP41009
Hello,
I need some help here with the choice of transformer I can use for this flyback converter (UCC28740) that can be able to step the input voltage to 15V, 2A and an input voltage of 1kV. WEBENCH gave me this transformer.
I'm wondering if my design would produce the same results if I used any of these transformers (ZB1432-CL) or (WA8759).
Please advise if there are any alternative transformers I can use apart from the one I specified.
Regards,
Ikenna.