Other Parts Discussed in Thread: TPSM8D6C24, TPSM8D6B24, TPSM8D6C24EVM-2V0, TPSM8D6B24EVM-2V0, USB-TO-GPIO2
Hi All,
I have question about TPSM41625.
A customer is considering using the TPSM41625 with a 5V output and a 50A load current.
For 5V output, load current up to 22A, so is 50A load current possible with 3pcs TPSM41625?
TPSM41625 (17A) x3pcs = 51A
Or, what other DCDC converters with built-in inductors do you recommend?
Best Regards,
Ishiwata