This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562209: About application report SLVA477B output voltage setting Equation 9

Part Number: TPS562209
Other Parts Discussed in Thread: TPS562200

Hi team,

About application report SLVA477B had mentioned that current IR1/2 needs to >100 times IFB.

But as TPS562209 datasheet mentions.

Output: 3.3V, R2=33.2K, R3=10K

IR1/2= 3.3/(33.2K+10K) = 0.0764 mA

But this didn't meet  >100 times IFB.

Why these two result can't meet?