Hi Team
1.According to "Functional Safety FIT Rate, FMD, and Pin FMA" Tabel4.2, the description of Pin 4(Vcc) short to GND is Fault mode will shut device off, but I set Up Vin 25V,output 5V, then short to Vcc Pin to GND, the IC damadge (sparks and smoke ), not match Tabel4.2 description.
2. The internal regaulator output protect is? (limit spec)
3.Vin 25V, then Vcc short to GND, the failure step is following below?
--> internal regaulator fail--> Low side MOSFET fail --> High side MOSFET fail --> continue supply power--> high energy at IC --> Over SPEC --> IC sparks and smoke ?
*The Power supply 25V,limit current: 12A