The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: Questions on application code programming

Part Number: TPS65982
Other Parts Discussed in Thread: TUSB546EVM

Hi,

I have some questions on the application code for PD Controller, TPS65982, used in TUSB546EVM.

Q1: There is a file "config82_A_v1.7.6_app_code.ctb", how do I use the file (.ctb)?

Q2: Do I use the TPS6598x Utilities GUI tool to download the binary files into the SPI flash? Or do I use the TPS6598x Application Customization Tool?

Q3: Why can't I import the setting from the config82_A_v1.7.6.json into the Application Customization Tool?

Q4: After I set the registers in the Application Customization Tool, do I save it to a binary file to be flash into the Low/High Region of the Flash memory later? When to choose to save as a Full Flash Image? 

Q5: From the memory organization, the config82_A_v1.7.6_low_region.bin is stored in the "App Code" memory space? 

Thanks.