Other Parts Discussed in Thread: LM61440
Hi,
I designed in the LM25145 using Power Designer. I need 12V input, 3.3V output and 4A. I copied the schematics almost exactly, except I used a 6.8uH vs the 6uH in the Power Designer and I put a 47uF (6.3V) and a 100uf (6.3V) cap, both ceramics as the datasheet states you can use low ESR caps on the output.
When I apply power, the output almost looks like the switching node. I don't like to turn it on too much because the noise greatly exceeds 3.3V. I then soldered a tantalum cap (68uF, 25V) and the supply works perfectly. I removed the tant and replaced with 2 more 100uF ceramics and the output shows the noise.
I have checked all component values thinking that maybe the CM installed a wrong value, but they are all good.
Do you have any idea why this circuit behaves this way?
Thanks,
JohnPowerSupply.docx