This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62870-Q1: Programming

Part Number: TPS62870-Q1

I see that the datasheet for the TPS62870-Q1 states that "Register contents remain intact as long as the input voltage remains above 1.4 V."

I was planning on using this device to generate a 0.9V rail.  Does the output voltage have to be re-programmed every time the device is powered?