Other Parts Discussed in Thread: LM66100
Hello,
My customer used the TPS82130 to power the supercap charge and buck/boost converter input with the following conditions.
- VIN = 5.6V, VOUT = 4.2V
When the input voltage of 5.6V is removed and the supercap is activated, a reverse current of about 1A occurs in the TPS82130.
Is this normal? Please let us know if there are any way to prevent the reverse current.
Thank you.
JH