I need to reduce the input and output capacitors for the TPS7H2211. For space applications, the datasheet uses 170uf for input and another 170uf for the output of the TPS7H2211. I have 1 TPS7H2211 output driving into 5 parallel TPS7H2211. The combined capacitive load for the input 12V PSU exceeds the PSU recommendation. What is the recommended minimum input and output capacitors for TPS7H2211? What is the risk of reducing the input/output capacitors? What is the rationale for using the high value capacitors?