Other Parts Discussed in Thread: BQ76PL455A
Hello to TI support team ,
I received expand Data sheet from TI according to bq79612 data , I have question according to Autonomous internal cell balancing mode :
1. Is this algorithm operate only in Charge or in Storage too ? (bq79612 is without system shunt so it doesn't have info according the current )
2. Can I set Threshold cell Voltage + Timer to operate and it will balance odd/even cells ?
3. The IC make balance to all the cells by default ?
4. What is the task of External Controller in Autonomous internal cell balancing mode ?
5. How the IC should react if an example all the cells 4.15V except one cell 3.6V --> What it the reaction of IC ?
6. During Shelf time (Storage ) disbalance starts increase --> How IC react ?
B.R
Alexander Burtakov