Hi Team,
my customer hope to achieve Vin rising threshold = 8V or 8.5V, Vin falling threshold = 5V or 4.5V.
But according to datasheet, min VIH=0.9V, max VIL=0.3V, so we should use this value for design, then above cannot be achieved. but typical VIH=0.9V, typical VIL=0.45V, the difference is not so large.
1. is there distribution data on VIH and VIL value? if the difference is not so large, maybe we can refer to the distribution to do design?
2. current threshold is to meet 1.8V I/O JEDEC requirement, right?
And internal circuit is just logic comparator circuit to set high and low threshold, right?
Thanks.
BRs
Given