Other Parts Discussed in Thread: LM74610-Q1, LM74700-Q1, , LM74700EVM
Hi,
Figure 12 (schematic) on pg. 16 shows using a single FET (SQJ422EP-T1-GE3) per path (FET1_A, FET2_A), which is rated 75A max - If I use 2 x of those FET's in parallel per path then the current rating would be double ~ 150A (2x 75A), right?
Figure 6 on pg.10 - What is the send voltage drop/dip after the FET has fully turned on

Thanks,
Tim