Part Number: TPS544B25
WE have been using the TPS544B25 for various out put voltages from 0.8/1.1/1.2/1.5/1.8/2.5/3.3/5.0V all with Rt=20.1K which is 1Mhz switching Freq. The tisp file to program the device was provided by the FAE. The same tisp file has been used for many board design with same circuit. Later we learnt that 100nS min PWM pulse width, then all the low vottage REGs need to run at low freq to meet the spec.
However, when the power supply was brought up using the same tisp file as it is agnostic to freq of operation, some of the REGs shutting down when powered up wtih Ton_max fault.
The only way to make the REG to work is by giving wide UV and OV protection setting and even Ton Delay increase. All these nothing to do with this fault either.
We wonder if there is any other setting in tisp file which we can tweak ?
Thanks
Sen